Tools

Siemens GreeceSiemens Greece

Site ExplorerSite Explorer
Close site explorer

Desigo V5.1: Energy-efficient, flexible and future-proof building automation

09 September 2013

The Siemens Building Technologies Division is launching Desigo V5.1. Desigo V5.1 is the first and currently the only building automation system to support state-of-the-art technologies such as BACnet/IPv6, the latest Microsoft operating systems Windows 8 and Windows Server 2012 as well as the AMEV 1 recommendations, which are becoming increasingly important in German-speaking countries. With the BACnet B-AWS (BACnet Advanced Workstation) profile, the associated management station Desigo Insight V5.1 is the first building automation management station to be certified under BACnet Revision 1.10.

Desigo V5.1 is the first building automation system to use the BACnet/IPv6 standard. Since the IP (Internet Protocol) addresses under the IPv4 standard have been exhausted, IPv4 will be replaced by IPv6 in the coming years. The BACnet/IPv6 standard allows future automation stations and operator units to be integrated into the IT structure via IP, thereby supporting entirely new applications in the “Internet of Things” of the future.

Existing Desigo installations can be upgraded to BACnet/IPv6 without any rewiring by using the Desigo V5.1 PXG3.. router. The proven BACnet/IPv4, BACnet/LonTalk and BACnet/MSTP communications protocols will continue to be supported in order to ensure compatibility with existing installations as well as with third-party devices and systems. As a result, Desigo V5.1 not only protects investments, but, thanks to BACnet/IPv6, is ready for the future.

Desigo V5.1 is the first building automation system on the market to fully implement the latest AMEV BACnet 2011 V1.1 recommendations. These recommendations for planning, building and operating different disciplines in public buildings are updated regularly by the German AMEV working group in order to promote the standardization of disciplines. Compliance with AMEV recommendations are now binding for public sector bids in German-speaking countries, and the AMEV guidelines are becoming increasingly important in other European countries as well.

Desigo TRA (Total Room Automation), the flexible and programmable room automation system, is a key component of the Desigo V5.1 system. In Version 5.1, additional KNX room operator units for wall mounting as well as new flush-mounted room sensors have been added to the Desigo TRA product range. The Desigo library of tested applications now contains new applications for air quality and demand-based ventilation (variable volumetric flow systems – VVS). With these system enhancements, Desigo TRA can now measure temperature as well as air quality and humidity in the room. The Desigo TRA product range includes new room operator units with or without display and control elements as well as the right sensors for any application.

With the BACnet B-AWS profile, Desigo Insight V5.1 is the first management station of a building automation system to be certified under BACnet Revision 1.10, which gives users additional control options. The B-AWS profile support also ensures better compatibility with the products of third-party manufacturers. Desigo Insight V5.1 is the very first building automation management station to run under the latest Microsoft operating systems Windows 8 (business versions) and Windows Server 2012 as well as SQL Server 2012.

The Desigo building automation system is part of Siemens’ Environmental Portfolio. In fiscal 2012, revenue from the Portfolio totaled about €33 billion, making Siemens one of the world’s largest suppliers of ecofriendly technologies. In the same period, our products and solutions enabled customers to reduce their carbon dioxide (CO 2 ) emissions by more than 330 million tons, an amount equal to the total annual CO 2emissions of Berlin, Delhi, Hong Kong, Istanbul, London, New York, Singapore and Tokyo.

1.Mechanical and Electrical Engineering Working Group of German National, Regional and Local Governments (www.amev-online.de)
 

The Siemens Infrastructure & Cities Sector (Munich, Germany), with approximately 90,000 employees, focuses on sustainable technologies for metropolitan areas and their infrastructures. Its offering includes products, systems and solutions for intelligent traffic management, rail-bound transportation, smart grids, energy efficient buildings, and safety and security. The Sector comprises the divisions Building Technologies, Low and Medium Voltage, Mobility and Logistics, Rail Systems and Smart Grid. For more information, visit www.siemens.com/infrastructure-cities

The Siemens Building Technologies Division (Zug, Switzerland) is the world leader in the market for safe and secure, energy-efficient and environment-friendly buildings and infrastructures. As technology partner, service provider, system integrator and product vendor, Building Technologies has offerings for safety and security as well as building automation, heating, ventilation and air conditioning (HVAC) and energy management. With around 29,000 employees worldwide, Building Technologies generated revenue of 5.8 billion Euro. For more information, visit www.siemens.com/buildingtechnologies