Siemens Greece

Site Search

Menuclose
Related
Info
close
Media Center

Media Center

The new ICE 3: More comfort for passengers

20 February 2014

Dr. Jürgen Wilder (left), CEO of the Siemens High-Speed and Commuter Rail Business Unit and Andreas Busemann (right), Head of Production at DB Bahn Long Distance, present Deutsche Bahn's new ICE 3 on a presentation run on the Frankfurt (Main) – Cologne line.

  • Siemens to deliver a total of eight new trainsets by the end of March

  • Smooth start for passenger service

Andreas Busemann, Head of Production at DB Bahn Long Distance, and Jürgen Wilder, CEO of the High Speed and Commuter Rail Business Unit of Siemens AG, presented the new ICE 3 of Deutsche Bahn (DB) today on a press tour.

“Above all, the new ICE 3 offers our customers a real plus when it comes to service and comfort. Passengers can keep informed about the train’s progress on the new overhead monitors, and comfortably dine in the full-sized onboard restaurant with 16 seats while traveling through Germany at speeds of up to 300 kilometers an hour. In addition, the Series 407 scores with lower energy consumption and higher technical reliability,” commented Busemann. 

In particular, the most modern ICE train offers numerous improvements for passengers with reduced mobility. The new trainsets are the first in Deutsche Bahn’s long-distance trains to provide a lift for wheelchair users. The wheelchair area is generously dimensioned, and both wheelchair spaces are fitted with a height-adjustable table and a service call button. A tactile guidance system including floor strips and tactile seat numbers helps sight-impaired and blind passengers. In addition, grab poles are provided in longer aisle sections, aisle seats have grab handles, and the door steps and inner doors are designed with stronger visible contrasts.

The Series 407 is based on Siemens’ Velaro platform. The new ICE 3 also has eight cars – like its forerunner – yet offers more seats: 444 including 111 in first class. Two trains can be coupled into a double unit with a seating capacity of 888. Externally, the new train differs from its forerunner through a newly designed front end and a front-to-rear raised roof section for improved aerodynamics.

In December 2013, the new ICE 3 was approved for double-unit operation within Germany. By the end of December 2013, four ICE trains were handed over to Deutsche Bahn. Four additional trains are to follow by the end of March 2014. “We have successfully mastered the challenges, in particular those presented by the certification process, and are pleased to see the new ICE 3 running on Germany’s lines,” said Wilder. 

Siemens is delivering a total of 17 trains to DB. At present, the first new ICE 3s are primarily running on the Cologne-Frankfurt (Main)-Stuttgart line in place of the previous ICE 3. Beginning in mid April, the eight delivered trains will be integrated into the current timetable. In coordination with DB, Siemens is conducting comprehensive test runs in France and Belgium with an additional eight trains in order to prepare for official approval of cross-border operation to these countries.

For further information, please go to: www.siemens.com/press/ICE

Siemens AG (Berlin and Munich) is a global powerhouse in electronics and electrical engineering, operating in the fields of industry, energy and healthcare as well as providing infrastructure solutions, primarily for cities and metropolitan areas. For over 165 years, Siemens has stood for technological excellence, innovation, quality, reliability and internationality. The company is one of the world’s largest providers of environmental technologies. Around 43 percent of its total revenue stems from green products and solutions. In fiscal 2013, which ended on September 30, 2013, revenue from continuing operations totaled €75.9 billion and income from continuing operations €4.2 billion. At the end of September 2013, Siemens had around 362,000 employees worldwide on the basis of continuing operations. Further information is available on the Internet at: www.siemens.com.


Like its predecessor, the new ICE 3 is composed of eight coaches, but offers more space with a total of 444 seats. With a rated traction power of 8,000 kilowatts (about 11,000 HP), it operates in Germany at up to 300 kilometers per hour.



You are changing from the tablet to the classic version. Do you want to proceed?