Tools

Site ExplorerSite Explorer
Close site explorer

Siemens Healthineers introduces next-generation RAPIDComm System

31 August 2016

  •  V6.0 delivers a total solution for POC data management with cardiac support via connectivity to the Stratus® CS 200 Acute Care™ Diagnostic System1

  • Offers performance and productivity enhancements to V5.0 including remote operator management, inventory management and time synchronization

Siemens Healthineers announced today it released a major software upgrade for the RAPIDComm Data Management System (V6.0), an informatics solution to centrally manage in vitro diagnostics analyzers and operators at the point-of-care (POC). In addition to the system’s enhanced productivity and performance features, RAPIDComm V6.0 now connects with POC cardiac devices.

“Point-of-care coordinators face tremendous workflow challenges when implementing and managing POC testing programs,” said Peter Koerte, President, Point of Care, Siemens Healthineers. “They are typically responsible for managing the testing done at dozens of locations on hundreds of devices and by thousands of operators, all while ensuring results are delivered quickly and reliably, and that compliance requirements of the laboratory remain satisfied.”

RAPIDComm V6.0 offers a complete solution for POC data management with the addition of cardiac support. With connectivity to the Stratus® CS 200 Acute Care™ Diagnostic System, the RAPIDComm system facilitates increased accessibility and oversight for point-of-care coordinators. System features such as the lock-out component—which prohibits operators not yet certified to use the equipment from running tests—are designed to improve compliance practices and enhance patient safety.2

With the introduction of several performance and productivity features, RAPIDComm V6.0 also reduces manual intervention and sneakernetting—or physical transmittal of data from one device to another. RAPIDComm system V6.0 integrates with multiple host connections and includes time synchronization with CLINITEK Status® Connect System, which automatically synchronizes the instruments daily for consistency across the point-of-care ecosystem.
RAPIDComm system V6.0 also introduces a new configurable backup utility, making it easier for customers with remote database configurations to directly manage their database backup activities.

Further, Material Use Reports for diabetes and urinalysis aid in inventory management, while Device Status alerts, email notifications and operator comments alert coordinators to when the instruments need attention.

For further information on the Siemens RAPIDComm Data Management System, please visit: www.siemens.com/rapidcomm.

1 Product has not yet been cleared for use in the U.S. Product availability varies by country.

2 Product has not yet been cleared for use in the U.S.

The products/features (here mentioned) are not commercially available in all countries. Due to regulatory reasons their future availability cannot be guaranteed. Further details are available from the local Siemens organizations.


Elisavet-Vasiliki Sachinidou 

 elisavet.sachindou@siemens.com