Site ExplorerSite Explorer
Close site explorer

Siemens Healthineers Unveils Game-changing Atellica Solution to Europe

07 November 2016

  • Patented, bi-directional magnetic sample transport technology1 is 10 times faster than conventional conveyors

  • Immunoassay analyzer delivers the industry’s highest productivity per square meter2—more than 400 tests per hour3

  •  Multi-camera vision system and intelligent sample routing enable independent control over every sample from routine to STATs1

  • Scalable up to 10 components and more than 300 customizable configurations1 can be used as a standalone system or connected to automation1

  • Can handle more than 30 sample container types including pediatric and special containers

Today Siemens Healthineers unveiled the Atellica™ Solution1, a highly flexible immunoassay and clinical chemistry solution featuring patented bi-directional magnetic sample-transport technology that is 10 times faster than conventional conveyors.1 The unveiling to the European market occurred during the Siemens Healthineers ‘Touching the Future’ Meeting in London, which was held on September 28th and 29th.

“We engineered the Atellica Solution1 based on our customers’ needs and extensive research of market trends,” said Franz Walt, President, Laboratory Diagnostics, Siemens Healthineers. “The result is a game-changer that delivers control and simplicity, so our customers can focus on driving better business and clinical outcomes and spend less time managing operations.”

In addition to the speed afforded by the Atellica Magline™ Transport technology,1 the Atellica Solution1 offers a multi-camera vision system1 and intelligent sample routing1 for independent control over every sample from routines to STATs.

The Atellica Solution1 provides unprecedented flexibility to adapt to growing testing needs and space constraints. The solution can be used as a stand-alone system, is scalable up to 10 components and can be combined into more than 300 customizable configurations,1 including L-shaped, U-shaped, and linear formations. It can also be connected to Aptio® Automation for a comprehensive, multidisciplinary solution.1 The solution can handle more than 30 sample container types including pediatric and special containers.

Further, the same reagents can be used across configurations and locations, simplifying laboratory operations, streamlining inventory control, and enabling consistent testing results. Additionally, a single immunoassay analyzer processes more than 400 tests per hour,3 delivering the highest productivity per square meter in the industry.2

Other benefits of the Atellica Solution1 include remote-access monitoring and control1 to maximize uptime, as well as a broad, expanding assay menu1 using proven detection technologies.

“The Atellica Solution offers us those technological tools that we have been waiting for such a long time,” said Dr. Josep Lluís Bedini, Head of the Core Lab Operative Area, Hospital Clínic Barcelona. “Our experience and expectations, as laboratory professionals, have been materialized in something real. We finally see something really new for the central laboratories that will fulfill our technical and workflow requirements.”

The Atellica Solution1 is the first in a new line of Atellica products engineered by Siemens Healthineers and further innovations are in the R&D pipeline.

1 Products are under development.  Not available for sale.  Any features listed are part of the development design goals.  Future availability cannot be guaranteed.

2 Versus leading IVD market competitors.

3 Dependent upon test mix.

For further information on Siemens Healthineers, please see

Elisavet-Vasiliki Sachinidou