Tools

Supply Chain ManagementSupply Chain Management

Technical Safety - Dangerous Goods

The aim of the dangerous goods regulations is also our goal:

To prevent - as far as possible - risks to persons or property and damage to the environment, the means of transport used or to other goods as far as possible.
Compliance with the dangerous goods regulations assures that risks will be eliminated or reduced to a minimum.

Safe transport of dangerous goods

Compliance with dangerous goods regulations is guaranteed by a worldwide network of properly trained employees throughout the complete transport chain - classification of our products, selection of transport mode, packing, shipping, use of service providers, etc. Our procurement and development departments are already focusing their attention on these regulations to assure our products can be transported worldwide in full compliance with the applicable legal requirements. As a global player, we also strive to serve our customers in this area in a safe manner without delay or objection.

Information for suppliers

Compliance requirements concerning the transport of dangerous goods

Shipments containing dangerous goods have to meet all the applicable dangerous goods requirements of the used transport modes and the relevant national variations, also depending on the chosen routes. The responsibilities for the different subjects - classification, allowed inner or outer packaging, mass and contents limits, marking, labelling, accompanying documents etc. -are regulated by the international and national dangerous goods regulations. Properly trained employees must be available in adequate numbers in the companies involved in dangerous goods transport in order to ensure that all relevant activities can be performed in compliance with the regulations.

Requirements towards our supplier

Our suppliers are required to ship dangerous goods in compliance with the dangerous goods regulations applicable for the goods and the transport mode ordered, with simultaneous consideration of relevant national or operator variations. This may also include additional requirements for permitted inner packaging for planned successional transports as given in an order which also have to be taken into account.

During the initial process of quotation, suppliers are required to provide data on the dangerous goods to ensure that:

  • dangerous goods will be identified even when contained in equipment

  • especially for components and assemblies which will be integrated into a product, the possibility of transporting the planned product can be checked by us at the earliest stage of development.

Conclusion of a contract with service providers

When making a contract with service providers (freight forwarders, packers etc.), the necessary dangerous goods information will be provided by the contracting entity at Siemens (also including affiliates) as required in the dangerous goods regulations.

Data delivery

The list of the dangerous goods data on which we need information is available in the Downloads. They may alternatively be given as part of a Material Safety Data Sheet containing all the necessary data if dangerous materials are concerned. For lithium cells or batteries - also packed with or contained in equipment – and for non-spillable, wet batteries – also contained for example in an uninterruptible power supply - the given forms (see Downloads) have to be used if the certification (specific for battery type and manufacturer) is not already available at Siemens.
According to our experience, the following points have to be kept in mind:

  • Some goods classified as dangerous goods may be transported as a complete or partial exception to the dangerous goods regulations of a specific carrier. This must not result in the classification "no dangerous goods" being given! The correct classification according to the dangerous goods regulations has to be given to ensure that goods can be properly classified for all transport modes used.

  • Lithium batteries may only be assembled from tested lithium cells and have to be tested according to the applicable battery tests (38.3 UN Manual of Tests and Criteria).

Contact and Downloads

If you have any questions regarding this subject, contact your Siemens partners. They will involve their competent safety adviser for the transport of dangerous goods, the competent division officer or the Corporate Office of Radiation Safety and Dangerous Goods as and when required.